STM32F217 and analog watch dog
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-11-07 9:40 AM
I use TIM8 for start of conversion and ADC_EXTERNALTRIGCONV_T8_TRG event for get a value of ADC in recycle mode with analog WDG. analog watchdog. I set both AWDIE and EOCIE. It work fine. An interrupt occurs every time in the end of conversion process. But i do not want it. I want to an interrupt occurred in case when ADC value will be higher or lower some level. If i reset EOCIE an interrupt does not occure never. AWD does not call an interrupt of ADC. Is it my mistake or it should be? May be there are an example with analog wath dog for HAL?
My config code is bellow. ADC_AnalogWDGConfTypeDef AnalogWDGConfig; ADC_ChannelConfTypeDef sConfig; /* ADC Initialization */ AdcHandle.Instance = ADC1; // AdcHandle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2; AdcHandle.Init.Resolution = ADC_RESOLUTION12b; AdcHandle.Init.ScanConvMode = DISABLE; AdcHandle.Init.ContinuousConvMode = ENABLE; AdcHandle.Init.DiscontinuousConvMode = DISABLE; AdcHandle.Init.NbrOfDiscConversion = 0; AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING; AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T8_TRGO; AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT; AdcHandle.Init.NbrOfConversion = 1; AdcHandle.Init.DMAContinuousRequests = ENABLE; AdcHandle.Init.EOCSelection = DISABLE; if (HAL_ADC_Init(&AdcHandle) != HAL_OK) { /* ADC Initiliazation Error */ Error_Handler(); }/**Configure the analog watchdog */ AnalogWDGConfig.WatchdogMode = ADC_ANALOGWATCHDOG_SINGLE_REG; AnalogWDGConfig.HighThreshold = 1500; //1,19V AnalogWDGConfig.LowThreshold = 500; //0,4V AnalogWDGConfig.Channel = ADC_CHANNEL_6; AnalogWDGConfig.ITMode = ENABLE; HAL_ADC_AnalogWDGConfig(&AdcHandle, &AnalogWDGConfig); /* Configure ADC1 regular channel */ sConfig.Channel = ADCx_CHANNEL; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; sConfig.Offset = 0; if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK) { /* Channel Configuration Error */ Error_Handler(); } #stm32f217-analog-watch-dog- Labels:
-
STM32F2 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-11-07 11:14 AM
Sorry Guys, it is my mistake. I has corrected HAL driver stm32f2xx_hal_adc.c and all work correct now.