2014-03-14 8:02 AM
1. Everything normal
2014-03-15 5:50 AM
Indeed, but I think the exercise here was to understand the observed behaviour, and where the stack size was defined.
Yes, being in main() would compound the issue, given that it never leaves and the stack allocation for the local/auto variables is thus rather permanent. In the general case however having several KB of stack space for temporary variables, and totally avoiding the use of dynamic allocation, or large global ones, is not necessarily unreasonable. Where issues really come up is when PC programmers, used to vast/endless stacks, allocate massive structures on the stack, or utilize recursion. It is important to consider stack depth, and call tree implications, and balance the use of global allocations against ones that are only temporal in nature.2014-03-15 11:41 AM
''Prefixing them with the ''static'' keyword will move them to the heap''
No, it won't.The heap is used by malloc() for dynamic allocation!''but bear in mind they'll keep their value through successive runs of the function''Correct.''That is to say, if function ''foo'' has a static int which it sets to 123, when it's run again, that value will be pre-set to '123' again''A point of clarification:If the value is set by the initialiser in the definition, it is only applied once - at startup. If the function then modifies the value, it is the modified value that will still be there the next time the function is entered.''As a bonus, the linker will complain if you try to allocate more variables than you have available heap memory''Again, the heap is used for runtime dynamic allocation - so the Linker can't warn about that. But it can warn about variables declared as 'static'.2014-03-17 12:37 PM
''To be honest, you really shouldn't be allocating variables as large as that on the stack''
Why not?''The total size of those is going to be several kilobytes!''Which is not a problem provided you have a suitably-sized stack...