cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103xC LQFP100 bootloader flash via ST link V2

Prince_Pk
Associate

Hai,

Im having a devention dev10 fpv controller, it is detecting by windows but not recognizing via Dfuse tools to flash its firmware to "Deviation". So I decided to flash bootloader via ST link V2 tool. Anyone please help me to get the STM32F103xC pin out config to connect to ST link V2 adaptor and its boot0 setting too.

 

Thanks in advance for your time and consideration.

1 REPLY 1
KDJEM.1
ST Employee

Hello @Prince_Pk and welcome to the Community ,

DfuSe is marked as NRND on its home page. For that please use STM32CubeProgrammer instead.

KDJEM1_0-1710320942627.png

To configure boot pin I recommend you to refer to RM0008 section 3.4 boot configuration.

KDJEM1_1-1710321094888.png

Also I advise you to take a look to MOOC - STM32 boot and startup tips - YouTube may help you.

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.