cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f103rbt6 Nucleof103 can bus not working

Hp.14
Associate II

Hi all,

can on the nucleo board is not working.

tried using HAL and bare metal.

could this be a hardware issue with connections on the nucleo board.

for ex. there is a limitation on usart2.

the same hal code with appropriate linker works fine for the bluepill.

and since both are based of the f103 platform... i was thinking it could an issue with the nucleo board.

associated link with some specifics

UPDATE 1:

i am soo royally screwed, any hints, leads to address the issue would be much appreciated

Kindly advise

0 REPLIES 0