2023-10-25 12:53 PM - edited 2023-10-25 04:55 PM
Hi,
I am quite new to STM32 MCU family and have a quick question. I attached schematic for the reference.
Is STM32F103CBT6 capable of driving complementary 50 kHz of PWM signals(HI and LO) with configurable duty cycle for the gate driver IC? Yes, I am aware that the chip has configurable PWM pins and it is possible to implement. But is it possible as a feedback controller? I am building a synchronous buck converter by using gate driver IC and STM32 as a feedback controller. Is there any limitation on the MCU itself that I need to be aware..? So far open loop without using STM32 is working on the board. Now I am trying to use MCU as a feedback controller but I am hearing some comments that it's impossible...
Any comments would be appreciated. Thank you
2023-10-27 12:03 PM
any help on this thread :(?