2018-08-20 5:47 AM
On the following page, the STM32F102xC row claims to have 64k sram.
However in the spec sheet, and in cubeMX i can only find 48k models. I expect the online table is wrong in this case.
2018-08-20 5:49 AM
Actually, in cube MX there is an RC model with 64k, but nothing in the spec sheet seems to imply this is possible. Have I missed something?
2018-08-20 5:51 AM
2018-08-20 5:53 AM
2018-08-20 6:15 AM
ST makes significantly fewer die options than packaging/marking would suggest.
Yes, definitely seems to be a lot of internal inconsistencies in info-graphic, tables and spec sheets. @STOne-32
RAM and FLASH sizes are readable via word locations in OTP/ROM