[STM32F103] CAN_RX0 and CAN_RX1 interrupts stop working if I power board using USB cable.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-23 2:33 PM
If powered otherwise, everything is OK.
HAL_CAN_RxFifo0MsgPendingCallback is CAN_RX0 and HAL_CAN_RxFifo1MsgPendingCallback is RX1 right?
I see that "USB low priority or CAN RX0 interrupts" are connected, but CAN RX1 should be independent from USB?
Is it possible to use CAN RX interrupts with USB plugged in (only for powering board)?
- Labels:
-
CAN
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-23 2:43 PM
Doesn't the STM32F103 share a common buffer between USB and CAN?
If you want the two functions to co-exist you'd need to be using F105 or F107 devices.
If you're not actually using the USB interface/pins, double check you're not setting some register bits, or disabling some clocks.
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
‎2022-03-31 6:05 AM
To continue on the hypothesis of @Community member​ , please refer to the article Concurrent use of USB and CAN with STM32F103.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.