cancel
Showing results for 
Search instead for 
Did you mean: 

Drone CAN Setup (STM32H753 -STM32F103 Flight Controller)

MShow
Visitor

Hello everyone

I'm new here, but i have worked on a flight controller unit FCU with those:

FMU Processor: STM32H753
IO Processor: STM32F103

This FCU then connected to a Raspberry Pi4, auxiliary, where  run his drone python software, using MAVlink approach for telemetry data and CAN communication and parameters setup;

Right now

We have a (good) software ready, with some wizard working well

BUT

we have an issue with CAN-motors and our STM chips...

Is it possibile that those H753 is NOT able to read a CAN motor ,brand new, out of fabric?

or better

Is the chip (H753) ABLE to write a NODE ID on a CAN motor, wich is ut of fabric (nodeID=1) to an actual working NODE ID(10,11,12 etc..)?

We had this issue....

based on your knowledge..
The correct way is to use a CAN-USB to "wake up" motors one by one and then connect to FCU?


Thank you


0 REPLIES 0