cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 - Can I use BOOT Pin as GPIO - EXTI Function?

valeriogiampa
Associate II
Posted on August 25, 2011 at 17:41

Hi,

I would like to know, if I can use a Boot pin of my STM32F103 how GPIO pin to monitor an EXTI event.

I have just used all other pin and I have necessity to use an additional external interrupt.

A Boot pin is a free pin used only for boot operation, but I don't know if I can program it for alternative function.

Best Regards

Valerio

1 REPLY 1
Posted on August 25, 2011 at 19:40

BOOT0 is not available to you

BOOT1 can be used as PB2
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..