2023-12-18 06:46 AM
Hello, I have a set of extended CAN ID's I need to pas the bxCAN filter. I looked at some examples where one ID is passed the filter, but could not figure out how to allow a set of ID's. If my understanding is correct the mask is used to determine which bits of the ID are important. How can I configure the filter so that I can pass a set of different ID's?
These are the ID's:
// 0x0CF00400
// 0x0CFD9200
// 0x18FEE500
// 0x18FEEE00
// 0x18FEEF00
// 0x18FEF200
// 0x18FEF700
// 0x18FEFC00
This is what my filter config looks like:
can_fil.FilterBank = 0;
can_fil.FilterMode = CAN_FILTERMODE_IDLIST;
can_fil.FilterFIFOAssignment = CAN_RX_FIFO0;
can_fil.FilterIdHigh = 0;
can_fil.FilterIdLow = 0;
can_fil.FilterMaskIdHigh = 0;
can_fil.FilterMaskIdLow = 0;
can_fil.FilterScale = CAN_FILTERSCALE_32BIT;
can_fil.FilterActivation = ENABLE;
can_fil.SlaveStartFilterBank = 13;
Solved! Go to Solution.
2023-12-18 07:04 AM
Hello,
I think for your case, ID mask is not suitable as there are many differences in your ID list mainly the first ones. But here you need to use ID list but you need more than one filter to configure. Each filter can set 2 IDs. So you need four 32-bit filters in your case.
This is an example of a filter configuring your first two IDs:
#define REMOTE_FRAME 0 /* If = 1 the frame should be a remote frame. If = 0 the frame will be a data frame */
#define EXTID 1 /* If = 0 the frame should be a frame with standard ID. If = 1 the frame should be a frame with extended ID */
#define ID1 0x0CF00400
#define ID2 0x0CFD9200
#define FILTER_ID ((ID1 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2)) // ID1 = 0x0CF00400 (FxFR1[31:0])
#define FILTER_MASK ((ID2 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2)) // ID2 = 0x0CFD9200 (FxFR2[31:0])
sFilterConfig.FilterMode = CAN_FILTERMODE_IDLIST;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = (FILTER_ID >> 16); // Filter ID2 LSB (FxFR2[0:15])
sFilterConfig.FilterIdLow = (FILTER_ID & 0xFFFF); // Filter ID1 LSB (FxFR1[0:15])
sFilterConfig.FilterMaskIdHigh = (FILTER_MASK >> 16); // Filter ID2 MSB (FxFR2[16:31])
sFilterConfig.FilterMaskIdLow = (FILTER_MASK & 0xFFFF); // Filter ID1 MSB (FxFR1[16:31])
2023-12-18 07:04 AM
Hello,
I think for your case, ID mask is not suitable as there are many differences in your ID list mainly the first ones. But here you need to use ID list but you need more than one filter to configure. Each filter can set 2 IDs. So you need four 32-bit filters in your case.
This is an example of a filter configuring your first two IDs:
#define REMOTE_FRAME 0 /* If = 1 the frame should be a remote frame. If = 0 the frame will be a data frame */
#define EXTID 1 /* If = 0 the frame should be a frame with standard ID. If = 1 the frame should be a frame with extended ID */
#define ID1 0x0CF00400
#define ID2 0x0CFD9200
#define FILTER_ID ((ID1 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2)) // ID1 = 0x0CF00400 (FxFR1[31:0])
#define FILTER_MASK ((ID2 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2)) // ID2 = 0x0CFD9200 (FxFR2[31:0])
sFilterConfig.FilterMode = CAN_FILTERMODE_IDLIST;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = (FILTER_ID >> 16); // Filter ID2 LSB (FxFR2[0:15])
sFilterConfig.FilterIdLow = (FILTER_ID & 0xFFFF); // Filter ID1 LSB (FxFR1[0:15])
sFilterConfig.FilterMaskIdHigh = (FILTER_MASK >> 16); // Filter ID2 MSB (FxFR2[16:31])
sFilterConfig.FilterMaskIdLow = (FILTER_MASK & 0xFFFF); // Filter ID1 MSB (FxFR1[16:31])
2023-12-18 11:18 PM
And how can I configure more filters at once?
2023-12-19 12:19 AM
As I said using several filters.
For each filter (new filter configuration) you need to increment .FilterBank:
sFilterConfig.FilterBank = 0; -> filter number 0
sFilterConfig.FilterBank = 1; -> filter number 1
sFilterConfig.FilterBank = 2; -> filter number 2 etc ..
2023-12-19 03:44 AM
I didn't understand it the first time. Now I understand and got it working. This is how I implemented it:
void CAN_filter_config(uint8_t filter_index, uint32_t ID, uint32_t MASK) {
CAN_FilterTypeDef sFilter_config; // Create a new filter config structure for each call
sFilter_config.FilterBank = filter_index;
sFilter_config.FilterMode = CAN_FILTERMODE_IDLIST;
sFilter_config.FilterScale = CAN_FILTERSCALE_32BIT;
sFilter_config.FilterIdHigh = (ID >> 16);
sFilter_config.FilterIdLow = (ID & 0xFFFF);
sFilter_config.FilterMaskIdHigh = (MASK >> 16);
sFilter_config.FilterMaskIdLow = (MASK & 0xFFFF);
sFilter_config.FilterFIFOAssignment = CAN_FILTER_FIFO0;
sFilter_config.FilterActivation = ENABLE;
if (HAL_CAN_ConfigFilter(&hcan, &sFilter_config) != HAL_OK) {
CAN_error();
}
}
Mask and ID filter
#define FILTER_ID1 ((ID1 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK1 ((ID2 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_ID2 ((ID3 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK2 ((ID4 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_ID3 ((ID5 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK3 ((ID6 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_ID4 ((ID7 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK4 ((ID8 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
2023-12-19 04:08 AM
Nice!
2023-12-19 04:12 AM - edited 2023-12-19 04:13 AM
But better balance the FIFO usage so the first 4 IDs will be received by FIFO0 and the second 4 IDs will be received by FIFO1. So let your API to select the FIFO number and add it as argument to your API to set this parameter:
FilterFIFOAssignment
2023-12-19 04:46 AM
What difference does this make for receiving the ID's?
2023-12-19 06:20 AM - edited 2023-12-19 06:21 AM
No difference in term of ID acceptance but the frame will be received by the FIFO of which the filter was assigned to.
sFilter_config.FilterFIFOAssignment = CAN_FILTER_FIFO0; -> the frame will be received by FIFO0
sFilter_config.FilterFIFOAssignment = CAN_FILTER_FIFO1; -> the frame will be received by FIFO1
In your function you're forcing the FIFO to FIFO0 while you can also use FIFO1 to offload FIFO0.
2023-12-21 06:46 AM
I tried adding more filters, because I need the following ID's:
#define ID9 (0x18EAFF00U)
#define ID10 (0x18EEFF00U)
#define ID11 (0x18ECFF00U)
#define ID12 (0x18EBFF00U)
For this I added more filters:
#define FILTER_ID5 ((ID9 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK5 ((ID10 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_ID6 ((ID11 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
#define FILTER_MASK6 ((ID12 << 3) | (REMOTE_FRAME<<1) | (EXTID <<2))
This is how I call them:
CAN_filter(0, FILTER_ID1, FILTER_MASK1, CAN_RX_FIFO0, &hcan);
CAN_filter(1, FILTER_ID2, FILTER_MASK2, CAN_RX_FIFO0, &hcan);
CAN_filter(2, FILTER_ID3, FILTER_MASK3, CAN_RX_FIFO1, &hcan);
CAN_filter(3, FILTER_ID4, FILTER_MASK4, CAN_RX_FIFO1, &hcan);
CAN_filter(4, FILTER_ID5, FILTER_MASK5, CAN_RX_FIFO1, &hcan);
CAN_filter(5, FILTER_ID6, FILTER_MASK6, CAN_RX_FIFO1, &hcan);
I can still receive the ID's of the first 4 filters, but the 5th & 6th are not making it. Why can't I get the other filters to work?