stm32f100rb uart reading or writing prblm
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-23 1:42 AM
hello , we re using stm32f100b ,we use uart1 just for hyperterminal printf,
we use uart2 with interrupts of reading we try a simple prgm for write a frame of 16 bytes to uart2 and we connect rx2 to tx2 to read our own writing just for test now ,my interrupts work very good when i read from out a barcode reader for exemple. but when i connect my own tx2 i dont got any thing !!! i controlled every thing many times ...no data .my flag doesnt raise up?? i tried all three possibilities for rx2 pullup pull down nopull no changing
clck is 8mhz we use discovery cart and both of them 9600 baudrate 8 data no parity 2stop bits
in main:
__HAL_UART_DISABLE_IT(&huart2, UART_IT_PE); // parity error interrupt
__HAL_UART_ENABLE_IT(&huart2, UART_IT_ERR); //frame error interrupt
__HAL_UART_ENABLE_IT(&huart2, UART_IT_RXNE);// Receive interrupt
because : HAL_StatusTypeDef HAL_UART_Receive_IT(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size) doesnt work at all !!!!! bloques the prgm ???
if(HAL_GPIO_ReadPin(GPIOA, BUTTON_Pin)==1)//USER BUTTON PUSHED sensd 16 bytes frames
{ DATA_FRAME_GDT[0]=254;//0xFE DATA_FRAME_GDT[1]=49;//1 DATA_FRAME_GDT[2]=53;//sdt 5 DATA_FRAME_GDT[3]=98;//'b' DATA_FRAME_GDT[4]=49;//'1'; DATA_FRAME_GDT[5]=50;//'2'; DATA_FRAME_GDT[6]=51;//'3'; DATA_FRAME_GDT[7]=52;//'4'; DATA_FRAME_GDT[8]=53;//'5'; DATA_FRAME_GDT[9]=54;//'6'; DATA_FRAME_GDT[10]=55;//'7'; DATA_FRAME_GDT[11]=56;//'8'; DATA_FRAME_GDT[12]=57;//'9'; DATA_FRAME_GDT[13]=11;//number of data DATA_FRAME_GDT[14]=7;//crc//942 mod 17 DATA_FRAME_GDT[15]=253;//0xFE HAL_UART_Transmit(&huart1,DATA_FRAME_GDT,16, 0xFFFF);//for hyperterminal HAL_UART_Transmit(&huart2,DATA_FRAME_GDT,16, 0xFFFF);//for gdt one blok sending 16 bytes at same time //for(i=0;i<16;i++)//{ //HAL_UART_Transmit(&huart2,(uint8_t *)&DATA_FRAME_GDT[i],1, 0xFFFF);//for gdt sending byte by byte//HAL_Delay(10);//}in the interrupt subroutine of file stm32fxx_it.c
void USART2_IRQHandler(void)
{ /* USER CODE BEGIN USART2_IRQn 0 *//* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);#define RXBUFFERSIZE 1
uint8_t aRxBuffer[RXBUFFERSIZE];
if (HAL_UART_Receive(&huart2, (uint8_t *)aRxBuffer, RXBUFFERSIZE,1) == HAL_OK)
{ barcode_store[barcode_char_num]= aRxBuffer[0]; barcode_char_num++; if(aRxBuffer[0]==253) { barcode_collected=1; barcode_char_num=0; }}
do you have any idea why i cannot read my own transmission????
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-23 5:18 AM
i solved some issue now i can use
HAL_UART_Receive_IT(&huart2,aRxBuffer,1);main:
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{ if(huart--->Instance==USART2) {barcode_store[barcode_char_num]= aRxBuffer[0];
barcode_char_num++; if(aRxBuffer[0]==10) { barcode_collected=1; barcode_char_num=0; } HAL_UART_Receive_IT(&huart2,aRxBuffer,1);//activtae the interrupt every time }}but stll can receiieve just barcode reader not from my own tx the sended of 16 bytes frame ???? very strange !!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-10 9:44 PM
Hi Tarhan, 'HAL_UART_Receive' contains some loops inside of itself so i don't think it is the right place to use it in a 'IRQHandler' function. You had better to use it in main loop.