2021-12-10 6:00 AM
Hello, for my personnal project I use a stm32F98 with the CAN peripheral activated.
First of all I have an issue with the configuraiton gave in the stm32f0_firmware example but if I set the GPIO_InitStruct.Pull to GPIO_NOPULL, I cannot have the INAK bit reset when going from initialization mode to Normal mode.
The solution to have it reset was to set GPIO_InitStruct.Pull to PullUp.
But then I had another issue : The peripheral do not receive/transmit any message.
When configured in LoopBack mode, it receives what it has just transmitted, so I assume that I have configured it well.
I've followed stm32f0_firmware example to configure bit timing and I have a 120ohm termination resistor right after the transceiver.
At this stage I really don't know what could cause this behaviour and I'm pretty lost..
2021-12-10 6:36 AM
In loop-back mode the speed settings are going to match, and you don't need a responding device on the bus.
No real data here to validate speed, clock, settings, or anything.
2021-12-10 6:47 AM
I'm using a CAN232 dongle ( http://www.can232.com/?page_id=72 ) to read/write message on the bus from the ocmputer. I've configured the dongle speed to 1Mbit/s.
My STM32f0 settings are :
/* USER CODE END CAN_Init 1 */
hcan.Instance = CAN;
hcan.Init.Prescaler = 4;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_5TQ;
hcan.Init.TimeSeg2 = CAN_BS2_6TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = DISABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
GPIO settings :
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(canHandle->Instance==CAN)
{
/* USER CODE BEGIN CAN_MspInit 0 */
/* USER CODE END CAN_MspInit 0 */
/* CAN clock enable */
__HAL_RCC_CAN1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**CAN GPIO Configuration
PA11 ------> CAN_RX
PA12 ------> CAN_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;//GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_CAN;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* CAN interrupt Init */
HAL_NVIC_SetPriority(CEC_CAN_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(CEC_CAN_IRQn);
/* USER CODE BEGIN CAN_MspInit 1 */
By the way I've tried to catch frames with an oscilloscope but nothing comes out of the MCU.. Even if the timing was not good, I should see frames coming out of the TX pin don't I?