cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F091 - Bitbanding

We are porting a piece of software from STM32F1 to a STM32F091.

One part of the software is using bit banding. But in the library heade is no definition for the bit danding area in the memory.

I fear bit banding is not supported by this special device? Is that correct?

1 ACCEPTED SOLUTION

Accepted Solutions

'F0 is based on Cortex-M0 core, which does not support bit-banding (the same applies to 'L0/Cortex-M0+, 'F7/'H7/Cortex-M7). You'll have to rewrite your code.

JW

View solution in original post

6 REPLIES 6

'F0 is based on Cortex-M0 core, which does not support bit-banding (the same applies to 'L0/Cortex-M0+, 'F7/'H7/Cortex-M7). You'll have to rewrite your code.

JW

Ozone
Lead III

AFAIK, Cortex M0 devices (i.e. the core) do not support bitbanding.

I would think twice before using it anyway. Support of peripheral access depends very much on vendors, and is hardly portable.

Yes, portability is an issue, but that's generally an issue in the mcu world, not only for this particular feature; so one has to be aware of it and the possible pitfalls all the time anyways.

> Support of peripheral access depends very much on vendors

Can you please extend on this?

JW

Pretty sure Fujitsu (whatever it is called now) Cortex M devices support bitbanding in the entire peripheral area.

ST does not.

Thank you for your answers.

We have the code already running on F1 and F2 derivates so this problem was unexpected.

I did not expect trouble with that feature - lesson learnded ;)

Leo

Ah I see, thanks.

(Fujitsu->Spansion->Cypress->soon_to_be_Infineon ;) )

While talking about competition, note that bitbanding is an optional component, and not all 'M3/'M4-based mcus chose to implement it - e.g. some of the Atmel (now MCHP) ATSAMs don't.

JW