cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F072RB part no unavailability.

STAR
Associate II

I am looking for STM32F072RB part no but currently it is out of stock and not available anywhere. 

Can somebody provide alternative part no which is available easily.

Please share the source details .

Any help would be helpful. 

Thank you. 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

You can use the find pin compatible chips feature in CubeMX to find an alternative, if one exists. It's going to depend on your pinout.

Here's a partial list, which again, may or may not be valid for you based on your pinout.

0693W00000AP3GbQAL.png 

Note also that "STM32F072RB" doesn't define a chip, since there are two different packages with that part number prefix.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

You can use the find pin compatible chips feature in CubeMX to find an alternative, if one exists. It's going to depend on your pinout.

Here's a partial list, which again, may or may not be valid for you based on your pinout.

0693W00000AP3GbQAL.png 

Note also that "STM32F072RB" doesn't define a chip, since there are two different packages with that part number prefix.

If you feel a post has answered your question, please click "Accept as Solution".
STAR
Associate II

Thank you TDK for your reply.