cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F070RBT Bootloading via USB

CWedg.1
Associate III

According to AN2606 section 12 we can use USB DFU bootloader as long we have HSE using a 24, 18, 16, 12, 8, 6, 4 MHz crystal. This is missing from section 3.3 of the datasheet. Is there a reason for this?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello 

Thank you for bringing this issue to our attention.

I confirm that we need to add USB DFU bootloader to the datasheet. I reported internally.

Internal ticket number: 171357 (This is an internal tracking number and is not accessible or usable by customers).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello 

Thank you for bringing this issue to our attention.

I confirm that we need to add USB DFU bootloader to the datasheet. I reported internally.

Internal ticket number: 171357 (This is an internal tracking number and is not accessible or usable by customers).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

liaifat85
Senior III

Thanks for pointing this out.