2016-12-12 6:00 AM
I'm currently using the STM32F051R8T6, 64 pin LQFP. Is the STM32F091RCT6 in the same package fully pin-compatible?
Thanks,
Paul♯♯♯
#stm32f091 #compatible #stm32f051Solved! Go to Solution.
2016-12-12 12:55 PM
Hi Paul,
No, those two products are not fully pin to pin compatible.
I advise you to download their datasheets and see the pinout differences on section 'Pinouts and pin descriptions'.
Best regards,
Lawliet.
If this answers your request, please press 'correct'
:)
.2016-12-12 12:55 PM
Hi Paul,
No, those two products are not fully pin to pin compatible.
I advise you to download their datasheets and see the pinout differences on section 'Pinouts and pin descriptions'.
Best regards,
Lawliet.
If this answers your request, please press 'correct'
:)
.2016-12-13 6:37 AM
Thanks. I looked at the pinout of the package I need, and found that they're close. PF5, PF6, PF7 are VSS/VDD pins on the '091. I only use Ports A/B/C, so with a simple board change, I can switch to this part, and get 4x the RAM. That should work out just fine.
2016-12-13 7:55 AM
Hi Paul,
Do not forget to connect the new VDD/VDDIO2/VSS pins.
And, your migtation to STM32F091 should be fine.
Regards,
Lawliet.