cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030K6T6 support touch library?

navid ansari
Associate III
Posted on December 12, 2016 at 12:00

hi

in this doc en.DM00210526.pdf there is no name of STM32F030K6T6 to know which pin is which Chanel of touch.

and in STM32F030K6T6.pdf there is no name of touch in pin configuration.

can i use touch library on this MCU?

#touch-sense #stm32f030k6t6
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Max
ST Employee
Posted on December 12, 2016 at 12:18

Hello,

There is no touch sensing controller TSC on the STM32F030xxx.

If you need the function, use the STM32F031xxx (no usb) or the STM32F032xxx (with USB).

see the table

http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32f0-series.html?querycriteria=productId=SS1574

Best regards,

Max

Posted on December 12, 2016 at 12:24

thanks.

can i use software solution?

if its yes where can i find touch library to use in software?

Posted on December 12, 2016 at 12:38

have a look at thispost:

https://community.st.com/0D50X00009XkZ8gSAF

Oliver Beirne
Senior
Posted on December 13, 2016 at 16:25

Hi

navidrct@gmail.com

I have moved this post to the

https://community.st.com/community/stm32-community/stm32-forum?sr=search&ampsearchId=1f075d14-1117-4f25-85a1-96ea3fb8cda9&ampsearchIndex=0

where product related questions are posted.

Thanks

Oli