cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F051 ADC and Multiple input

SGian.1
Senior

Hi there !

I'm gonna use this microcontroller for one project. I start with configurate one ADC channel and i have a couple of question to ask .

1) More voltage input is close to Vref and more the value i read is close a the input ex: input 2.50 V i read 2.65V but if i have one input like 0.80V i read 1.15V

How can i fixed this problem ? right now i use the discovery board and i have a power supply for my ADC input

2) I try to confure other ADC pin but how if i have continus convers mode how i can know what kind of input i gonna read ?

Thank you soo much

Sergio

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AScha.3
Super User

1 -> did you run "ADC calibrate" ?

2 -> sequence (INT enabled) gives you interrupts after each conversion and end of sequence.

If you feel a post has answered your question, please click "Accept as Solution".
SGian.1
Senior

Yes i try to calibrate but still the problem. I try to read the ADC_CHANNEL_VREFINT but i received 0x0FFF and i don't know why. I think the problem is Vref right now my discovery is connected a the USB port. Today i try whit a external ADC and work perfect but i think is stupid use external ADC when this microcontroller have 16 ADC inside. And i misure the same voltage with the same power supply. Another thingh is i use 239.5 Cycles with the STM32F051.

I hope some one help me to understand

Thanks Sergio

raptorhal2
Lead

i use the discovery board and i have a power supply for my ADC input

Perhaps there is a ground difference between discovery and ADC input.

how i can know what kind of input i gonna read ?

For more than one channel, either the ADC needs to be reconfigured after each conversion for the next channel, or DMA must be used to move the ADC register data to your selected memory storage location after each conversion. There should be a DMA example in the examples that come with the library.

Cheers, Hal