cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5MMG with Full BLE stack / Power Consumption

Colpitts
Associate

Hi All,

I'm currently using an STM32WB5MMG on my project and I'm struggling to reach the expected power consumption.

Please note one known error on the PCB: the RF_OUT and ANT_IN pins, which should be connected to GND according to the datasheet/guidelines, were inadvertently left unconnected. These pins are currently inaccessible for rework.

Anyway, I'm trying with all the examples available for this MCU, and I have read all the conversations about this MCU and the Low Power modes multiple times with no success.

I have tested the PCB with the HeartRateFreeRTOS example and with the PWR_STOP2_RTC example, but again, no luck.

The current is always around 500 μA.

I have already tried to desolder all the sensors from the PCB to be sure that the extra consumption doesn't come from one of them, but no luck.

I have also deactivated all debug functionality while testing for power consumption, and I have tested the PCB with the debugger disconnected, so it is not related to this.

I also tried to initialize all the GPIO as ANALOG input as suggested in some posts (in PWR_STOP2_RTC, it was already done, so this is not the problem)

 

My First question is:" Could the missing connection to GND of RF_OUT and ANT_IN cause the extra consumption ?" I have no way to test this because those pins are not reachable to try to do a rework.

 

Second question: If this is not the issue, is there any known problem that could lead to this anomalous consumption?

Thanks
Jonny 

0 REPLIES 0