2018-05-18 03:01 AM
Turvey.Clive.002
‌Barkin.Tyler.001
‌Hi Clive ,
I'm using the STM32F072 discovery board. In that i'm using the CAN peripherals CAN_Tx and CAN_Rx .
Below is the circuit diagram of my connection.
I'm using MCP2551 trans-receiver. when i'm trying to send the CAN frame i'm getting the ''bit dominant error''.
I have monitored the CAN_ESR (CAN error status register) in that Last error code (LEC) i got the count 101=> which indicates the ''Bit dominant error''. I'm not understanding the what goes wrong , i have shared the code also please help me if any body is having the solution for this.
CODE
---------------------------------------------------------------
/* Includes ------------------------------------------------------------------*/
&sharpinclude ''stm32f0xx.h''/** @addtogroup STM32F0_Snippets
* @{ *//* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/&sharpdefine CMD_TOGGLE (0xDA)&sharpdefine CAN_ID_MASK (0xFF70U)&sharpdefine CAN_ID1 (0x651U)&sharpdefine CAN_ID2 (0x652U)&sharpdefine FILTER_LIST (1) /* 0: filter mode = identifier mask, 1: filter mode = identifier list *//* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*//* Private function prototypes -----------------------------------------------*/void Configure_GPIO_LED(void);void Configure_GPIO_CAN(void);void Configure_CAN(void);void Configure_GPIO_Button(void);void Configure_EXTI(void);/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program. * @param None * @retval None */int main(void){Configure_GPIO_LED();
Configure_GPIO_CAN(); Configure_CAN(); Configure_GPIO_Button(); Configure_EXTI();/* Infinite loop */
while (1) { }}__INLINE void Configure_GPIO_LED(void){ /* Enable the peripheral clock of GPIOC */ RCC->AHBENR |= RCC_AHBENR_GPIOCEN; /* Select output mode (01) on PC8 and PC9 */ GPIOC->MODER = (GPIOC->MODER & ~(GPIO_MODER_MODER8 | GPIO_MODER_MODER9)) \ | (GPIO_MODER_MODER8_0 | GPIO_MODER_MODER9_0);}__INLINE void Configure_GPIO_CAN(void){ /* Enable the peripheral clock of GPIOA */ RCC->AHBENR |= RCC_AHBENR_GPIOAEN; /* GPIO configuration for CAN signals */ /* (1) Select AF mode (10) on PA11 and PA12 */ /* (2) AF4 for CAN signals */ GPIOA->MODER = (GPIOA->MODER & ~(GPIO_MODER_MODER11 | GPIO_MODER_MODER12))\ | (GPIO_MODER_MODER11_1 | GPIO_MODER_MODER12_1); /* (1) */ GPIOA->AFR[1] = (GPIOA->AFR[1] &~ (GPIO_AFRH_AFRH3 | GPIO_AFRH_AFRH4))\ | (4 << (3 * 4)) | (4 << (4 * 4)); /* (2) */}/**
* @brief This function configures CAN. * @param None * @retval None */__INLINE void Configure_CAN(void){ /* Enable the peripheral clock CAN */ RCC->APB1ENR |= RCC_APB1ENR_CANEN; CAN->MCR |= CAN_MCR_INRQ; /* (1) */ while((CAN->MSR & CAN_MSR_INAK)!=CAN_MSR_INAK) /* (2) */ { /* add time out here for a robust application */ } CAN->MCR &=~ CAN_MCR_SLEEP; /* (3) */ // CAN->BTR |= CAN_BTR_LBKM | 2 << 20 | 3 << 16 | 5 << 0; /* (4) */ CAN->BTR |= 2 << 20 | 3 << 16 | 5 << 0; /* (4) */ CAN->MCR &=~ CAN_MCR_INRQ; /* (5) */ while((CAN->MSR & CAN_MSR_INAK)==CAN_MSR_INAK) /* (6) */ { /* add time out here for a robust application */ } CAN->FMR = CAN_FMR_FINIT; /* (7) */ CAN->FA1R = CAN_FA1R_FACT0; /* (8) */&sharpif (FILTER_LIST) CAN->FM1R = CAN_FM1R_FBM0; /* (9) */ CAN->sFilterRegister[0].FR1 = CAN_ID2 << 5 | CAN_ID1 << (16+5); /* (10) */ &sharpelse CAN->sFilterRegister[0].FR1 = CAN_ID1 << 5 | CAN_ID_MASK << 16; /* (11) */&sharpendif /* FILTER_LIST */ CAN->FMR &=~ CAN_FMR_FINIT; /* (12) */ CAN->IER |= CAN_IER_FMPIE0; /* (13) */ /* Configure IT */ /* (14) Set priority for CAN_IRQn */ /* (15) Enable CAN_IRQn */ NVIC_SetPriority(CEC_CAN_IRQn, 0); /* (16) */ NVIC_EnableIRQ(CEC_CAN_IRQn); /* (17) */}__INLINE void Configure_GPIO_Button(void){ /* Enable the peripheral clock of GPIOA */ RCC->AHBENR |= RCC_AHBENR_GPIOAEN; /* Select mode */ /* Select input mode (00) on PA0 */ GPIOA->MODER = (GPIOA->MODER & ~(GPIO_MODER_MODER0));}/**
* @brief This function configures EXTI. * @param None * @retval None */__INLINE void Configure_EXTI(void){ SYSCFG->EXTICR[0] = (SYSCFG->EXTICR[0] & ~SYSCFG_EXTICR1_EXTI0) | SYSCFG_EXTICR1_EXTI0_PA; /* (1) */ EXTI->IMR |= EXTI_IMR_MR0; /* (2) */ EXTI->RTSR |= EXTI_RTSR_TR0; /* (3) */ NVIC_SetPriority(EXTI0_1_IRQn, 0); /* (4) */ NVIC_EnableIRQ(EXTI0_1_IRQn); /* (5) */ }/******************************************************************************/
/* Cortex-M0 Processor Exceptions Handlers *//******************************************************************************//**
* @brief This function handles NMI exception. * @param None * @retval None */void NMI_Handler(void){}/**
* @brief This function handles Hard Fault exception. * @param None * @retval None */void HardFault_Handler(void){ /* Go to infinite loop when Hard Fault exception occurs */ while (1) { }}/**
* @brief This function handles SVCall exception. * @param None * @retval None */void SVC_Handler(void){}/**
* @brief This function handles PendSVC exception. * @param None * @retval None */void PendSV_Handler(void){}/**
* @brief This function handles SysTick Handler. * @param None * @retval None */void SysTick_Handler(void){}/** * @brief This function handles EXTI 0 1 interrupt request. * @param None * @retval None */void EXTI0_1_IRQHandler(void){ EXTI->PR |= 1; if((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0)/* check mailbox 0 is empty */ { CAN->sTxMailBox[0].TDTR = 1; /* fill data length = 1 */ CAN->sTxMailBox[0].TDLR = CMD_TOGGLE; /* fill 8-bit data */ CAN->sTxMailBox[0].TIR = (uint32_t)(CAN_ID1 << 21 | CAN_TI0R_TXRQ); /* fill Id field and request a transmission */ } else { CAN->TSR |= CAN_TSR_ABRQ0; /* abort transmission if not empty */ }}/**
* @brief This function handles CAN interrupt request. * @param None * @retval None */void CEC_CAN_IRQHandler(void){ uint32_t CAN_ReceiveMessage = 0;if((CAN->RF0R & CAN_RF0R_FMP0)!=0)/* check if a message is filtered and received by FIFO 0 */
{ CAN_ReceiveMessage = CAN->sFIFOMailBox[0].RDLR; /* read data */ CAN->RF0R |= CAN_RF0R_RFOM0; /* release FIFO */ if((CAN_ReceiveMessage & 0xFF) == CMD_TOGGLE) { GPIOC->ODR ^= GPIO_ODR_8; /* Toggle orange LED */ } }}/** * @} */@@@@@@@@@@null2018-05-24 09:15 AM
Hello,
I am not sure if
MCP2551 is a CAN transceiver, which can work with STM32 MCUs.
I saw many CAN buses with MCP2551, but these CAN
transceivers were connected to 5V MCUs, which in fact means that MCU's and tranceiver's CAN_RX and CAN_TX logic was 5V.
I saw also many CAN buses with STM32 MCUs, but here always CAN transceivers were also supplied with the same voltage as MCUs. For example all STM32 eval boards use TI's SN65HVD230 3.3V CAN tranceivers. As a result both MCU and CAN transceiver are supplied with 3.3V and their CAN_RX and CAN_TX logic is 3.3V.
In your design you use STM32F072, which can be supplied up to 3.6V and MCP2551, which is supplied with 5V. I would propose to double check that these devices can work together.
Regards
Szymon2018-05-24 10:45 AM
Where did you set ABOM ?
make sure that the two boards cannot transmit the same MsgID.
2018-05-24 11:20 PM
Thanks
Szymon for reply.
I got solution for my issue. Issue was not the 5volt or 3.3 volt supply.
Issue was i'm using the PA11 and PA12 pin for CAN_Rx and CAN_Tx i checked the schematic, i found that to access the PA11 and PA12 pin i need to short the SB link i.e SB20 and SB23 on the board.
Now its working fine. Thanks for your time buddy.
2018-05-24 11:21 PM
Thanks T J
for reply.
I got solution for my issue. Issue was not the 5volt or 3.3 volt supply.
Issue was i'm using the PA11 and PA12 pin for CAN_Rx and CAN_Tx i checked the schematic, i found that to access the PA11 and PA12 pin i need to short the SB link i.e SB20 and SB23 on the board.
Now its working fine. Thanks for your time buddy.