2018-05-10 10:10 PM
Greetings People,
I want to interface 6 common anode 7 segment display with my STM32F030R8. Any idea on schematic ? I have interfaced it with 8051 but and i have used Max7219 with STM32F030R8.
I don't want to go for Max7219 because dude to any noise in power line my Max7219 stops working.
Any guidance will be helpful thanks.
#7-segment-display #7-segment-display-multiplexing2018-05-10 11:26 PM
Yes, the 8051 was a bit flakey with any length reset line.
The STM32 chips are much more robust and stable.
There are more economical solutions over the Max chip, like
I used discrete components before, to save more money, how many pieces do you need to make ?
ie. ULN2003
and another transistor array for the digit select drive.