2018-03-12 12:32 PM
Whenever you want to update something you get:
I see also this problem when trying to open a project from v4.24.0, and when generating new project for an IDE.
In those cases the message is slightly different but still about problems with server connectivity.
2018-03-12 12:43 PM
Checked:
- 'no proxy' at home, and proxy at work
- 'check connection' button works fine (is GREEN)
- when you try to check update the 'check connection' becomes RED
2018-03-13 1:26 AM
I also have this problem ...
2018-03-13 1:37 AM
so much to just write a break
:(
2018-03-13 2:31 AM
Good to hear it! I was afraid that I am the only one...
2018-03-13 11:09 AM
Just tested it again and the server is available now. What about you?
2018-03-14 1:23 AM
Good. It worked...
2018-03-14 2:29 AM
It seems like the issue on the ST Server side...