cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L476 DAC usable range and ADC offset

Dan Hunter
Associate II
Posted on March 13, 2018 at 17:20

Using the Nucleo-L476RG development board for code development for a design prototype. What is the expected linear range of the DAC?

  • For the linear range, I am measuring the lower bound of the DAC about 55mV and upper bound about 3.271V.

  • Below and above this range the DAC rails. Vref (pin AVDD) is measured at 3.3191V.

  • This testing implies that the usable DAC range is approximately 70 counts to 4030 counts with resolution of 0.81mV/cnt (i.e. 3.319/4096 ... or 0.806mV/cnt if 3.3/4096), no?

If I execute the 'ADC_SingleConversion_TriggerSW_IT' program, the following DAC values are used (per comments in code)

/* Set DAC output on 5 voltage levels, successively to: */

/* - minimum of full range (0 <=> ground 0V) */

/* - 1/4 of full range (4095 <=> Vdda=3.3V): 1023 <=> 0.825V */

/* - 1/2 of full range (4095 <=> Vdda=3.3V): 2048 <=> 1.65V */

/* - 3/4 of full range (4095 <=> Vdda=3.3V): 3071 <=> 2.475V */

/* - maximum of full range (4095 <=> Vdda=3.3V) */

What I obtain: 

DAC CNT|uhADCxConvertedData|uhADCxConvertedData_Voltage_mVolt|Measured DAC (LeCroy)

   0   |       0           |                 0V              |      55.4mV

1023   |     983           |              793mV              |       850mV

2048   |    2011           |             1.619V              |      1.680V

3071   |    3035           |             2.444V              |      2.500V

4095   |    3994           |             3.218V              |      3.271V

  • The calculated DAC voltage (from ADC) is approx 56mV in error compared to measured DAC voltage.

  • Is this an offset within the ADC and can this be calibrated out internally via HAL/MIX/LL calls or do I have to write an ADC calibration routine?

Issue: I am doing motor control and need to use an external Vref as a basis. The offsets in the DAC and ADC need to be calibrated out and the linear range of each conversion (DAC and ADC) is required

#stm32l476-dac #stm32l476-adc
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User
Posted on March 13, 2018 at 19:03

What is the DAC load? DAC output buffer is on? Do your results depart from what's given in the DAC characteristics table in DS?

ADC offset is supposed to be nulled by calibration to be performed before first conversion, see Calibration (ADCAL, ADCALDIF, ADC_CALFACT) subchapter of ADC chapter in RM.

JW

Dan Hunter
Associate II
Posted on March 13, 2018 at 20:32

  • I am using the 

    ADC_SingleConversion_TriggerSW_IT example provided in en.stm32cubel4.zip

  • No load on the DAC - developing code at this moment. In the application, the DAC will be connected to an analog input of an H-Bridge. The analog

    input is used for the PWM control of the current loop. Need to monitor Vref of the H-Bridge via ADC to eliminate any offsets going into the comparator of the PWM control section. On the Nucleo-L476RG board, I removed SB21 so the LED is not loading the buffered output of DAC2
  • In the

    ADC_SingleConversion_TriggerSW_IT 

    example, DAC output buffer is enabled and the

    buffer

    is railing. Would like to know what are considered typical margins that I need to include. Per spec, it gives 200mV for each rail (200mV -> 3.1mV) at 25C I assume. To insure a 4-sigma that the DAC output is not hitting a 

    buffer

    rail (min/max limit) is 200mV sufficient??

         /* Configuration of DAC channel */

         sConfig.DAC_Trigger = DAC_TRIGGER_NONE;

         sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;

      From Spec:

         VDAC_OUT - Voltage on DAC_OUT output: 

            DAC output buffer ON:  (min) 0.2,  (max) VREF+ â€“ 0.2 V

            DAC output buffer OFF: (min) 0, (max) VREF+
  • In the example, the ADC is internally connected to the DAC. Is the ADC connected before or after the buffer? It appears after the buffer

  • The

    ADC_SingleConversion_TriggerSW_IT 

    example does not perform an ADC calibration. HAL_ADCEx_Calibration_Start() is no where to be found in the example's project. I'll add HAL_ADCEx_Calibration_Start() to the example and use HAL_ADCEx_Calibration_GetValue() to see what offset was calculated and if this improves the ADC values obtained.
  • For the DAC values of 1023, 2048 and 3071 and AVDD = 3.319, the DAC outputs should be 0.829V, 1.66V and 2.49V. I measured 0.850V, 1.68V and 2.50V respectively. Some offset at lower DAC values that needs further investigation. Used factory DAC offset for these tests

Posted on March 13, 2018 at 20:43

Jan

For readability for those who may follow this thread, DS is for DS10198 (DocID025976 Rev 5) and RM is for RM0351, no?

Posted on March 13, 2018 at 21:26

  • I added 

    HAL_ADCEx_Calibration_Start() to example 

    ADC_SingleConversion_TriggerSW_IT.

  • Using HAL_ADCEx_Calibration_GetValue(), the calibrated offset was 62. The results obtained below are more aligned

DAC CNT|uhADCxConvertedData|uhADCxConvertedData_Voltage_mVolt|Measured DAC (LeCroy)

   0   |      50           |               40mV              |      55.4mV

1023   |    1045           |              842mV              |       850mV

2048   |    2073           |             1.670V              |      1.680V

3071   |    3099           |             2.497V              |      2.500V

4095   |    4057           |             3.269V              |      3.271V

Two comments regarding User Manual UM1785 (Description of STM32F0 HAL and low-layer drivers)

  • On page 100 of UM1785, rev 6

    • 7.1.2 Detailed description of functions

      • HAL_ADCEx_Calibration_Start Function

        • HAL_StatusTypeDef HAL_ADCEx_Calibration_Start (ADC_HandleTypeDef * hadc)

      • ==> is INCORRECT!!! Should be:
        • HAL_StatusTypeDef HAL_ADCEx_Calibration_Start(ADC_HandleTypeDef* hadc, uint32_t SingleDiff)

  • 'HAL_

    ADCEx_Calibration_GetValue()' 

    is used in UM1785 for examples of APIs but NO

    description

     block 

    is given for this function! The same is also true for '

    HAL_

    ADCEx_Calibration_SetValue()'. I grabbed the following from file stm32l4xx_hal_adc_ex.c

    • uint32_t HAL_ADCEx_Calibration_GetValue(ADC_HandleTypeDef* hadc, uint32_t SingleDiff)

    • HAL_StatusTypeDef HAL_ADCEx_Calibration_SetValue(ADC_HandleTypeDef* hadc, uint32_t SingleDiff, uint32_t CalibrationFactor)

Posted on March 14, 2018 at 10:05

For readability for those who may follow this thread, DS is for DS10198

 (

DocID025976 Rev 5) and RM is for RM0351, no?

Probably yes - I am lazy to look up the numbers for your particular mcu model... ;)

Generally, these data are (or should be) in the respective datasheets and reference manual for all STM32 (although the ADC calibration applies only to some of them).

If you need some assurance for the values in the DS, I'm afraid you'd need to contact ST directly.

JW

PS. Just to make this sure: you've set the respective pin to Analog mode in GPIO and made sure pullup/pulldown is switched off - you can verify by reading back and checking the relevant GPIO registers

Posted on March 14, 2018 at 10:17

Dan,

I don't use the L4 and a brief glance at the DAC chapter in RM0351 reveals that it's way more complex than the one in the 'F4 I'm using.

Worth a thorough reading (as chapters for every other peripheral you may be using).

E.g.

In the example, the ADC is internally connected to the DAC. Is the ADC connected before or after the buffer?

is probably answered in DAC channel modes -> Normal mode (i.e. it is selectable)

JW