2017-01-24 10:55 AM
Hello all,
I am running into a problem with updating the STM32F4 library in STM32CubeMX ver 4.19. I want to install the STM32F4 library package ver 4.14. However, I get an error stating 'These Files have problem during Download : stm32cube_fw_f4_v1140.zip (Target directory already exists)'
I am able to install the previous STM32F4 package, rev 1.13 without problems.
I have tried uninstalling, reinstalling, deleting the repository package directory, etc, etc. No dice. Perhaps I am missing a directory to clean up while reinstalling. Also, I can see where the .zip is downloaded to when running the updater. There is nothing there. It shouldn't have any problems. I also tried installing the package via the 'Load from file', but no dice there. I get an error that way too.
I also thought that the package may have already come with CubeMX, but I am prompted to download the package when I try to generate code.Of course, this fails for the same reason
So, long story short, I am stuck. I would appreciate the help! Looks like there are others who have had issues in the past, but there are no answers.I listed on below.
https://community.st.com/0D50X00009Xkh43SAB
nullSolved! Go to Solution.
2020-04-13 06:42 AM
2020-05-21 12:26 PM
I had the same problem So, I uninstalled and deleted ALL ST stuff. It then would not install. It told me I had to uninstall first. ???
2020-05-21 12:27 PM
Can we just have an installer that works, and installs stuff that works?
2020-06-18 04:51 AM
This problem persists and applies to any repo unzip for any stm32cube product. Problem is interference with McAfee antivirus. Blocking antivirus fixes problem as a workaround, but I generally think it is a bad idea to do that while downloading files from internet...
ST need to se over the installer to be more friendly to antivirus...
Regards
/Peter
2021-02-20 02:31 AM
Hello all,
I've the same problem. I'm working with:
I've installed the last MCU Package for the STM32WB:
But when I try to import an example, I've the following error:
I've followed all previous suggest without resolve problem. How can I resolve this issue?
2021-02-20 02:36 AM
2021-07-21 10:20 AM
I think this is a very simple issue.
Briefing: