cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX - Power Consumption Calculator

mr2399
Associate
Posted on September 02, 2016 at 13:38

Hi,

is there the possibility to change the ''Vdd Power Supply'' values inside of the Parameter Selection. I would like to select 2.8V but doesn't have the possibility to do so. Also small file hacks are welcome...

Thanks in advance.

2 REPLIES 2
Nesrine M_O
Lead II
Posted on September 02, 2016 at 17:08

Hi banjoBazooka,

The power consumption calculator (PCC) in STM32CubeMX returns Average of current consumption, Battery life… these data are taken from the MCU datasheet or interpolated from a user specified bus or core frequency.

VDD parameter is fixed according to VDD values presented on datasheets.

Otherwise I will raise this request to our MX team as enhancement.

-Syrine-
Bino
Senior
Posted on September 05, 2016 at 09:53

Hello,

Could you please tell us the MCU Name you are using?

Thanks

/Eric