2018-03-06 01:33 AM
Why Stm32CubeMx doesn't work with Java 9 (9.0.4)?
I can't use Java 8 for some reason. Many other useful applications like eclipse are compatible with the newest Java version.
2018-03-12 02:45 AM
Hello
Sierzega.Andrzej
,Which CubeMx version are you using ?Could you please precise in details your OS environment (Linux, Windows..) ?
May be you can try uninstallingany installed version of Java before to install the new one, as the new installation of java doesn't automatically replace the old installations.
Best Regards
Imen
2018-03-12 04:25 AM
Hello Imen,
I installed the lastest version of CubeMx. I use Windows 10.
Using Java version 8 I have no problem with CubeMx. When I fully uninstall Java 8 and install only Java 9 I'm getting such error:
This problem can be solved only by programmers of CubeMX by compiling it for using Java 9. This problem is known for every software developers that must support new java version.
My version of Java is:
Regards
Andrew
2018-04-28 12:45 PM
I have same issue,
system Win10 64-bit,
`jdk-10.0.1_windows-x64_bin` installed on fresh system (so no other Javas installed),
`SetupSTM32CubeMX-4.25.0`
and same error message :\
2018-05-07 08:33 AM
Hi
Sierzega.Andrzej
,STM32CubeMX doesn't support Java9 for the moment.You can use java8.
Regards,
Houda
2018-05-13 07:52 AM
I also am having this issue, can not run Eclipse Oxygen.3 and
STM32CubeMX
on the same Java version. Hard Java version requires multiple Java installs, not advised. Please address.
2018-10-20 07:01 AM
I would like to refresh this thread. Please, build the software with the newest JDK possible, currently version 10. It is very confusing, the software doesn't run and complains about missing JRE 7. It works also with JRE 8, but not with 9 nor 10.
Thank you,
David
2018-11-28 01:27 PM
I use java8. It does not work!
2018-11-28 04:00 PM
here's a better suggestion - bundle the appropriate JRE with the application, like many other developers do.
2018-11-29 01:34 AM
I'm just trying to run the installation. What kind of application is it that he needs to dance with a tambourine to install it? I dont know where to search for java7. Installation redirects me to java8 page.