2024-07-05 11:12 AM - edited 2024-07-06 06:17 AM
Hi,
I am developing software on the stm32h743 using threadx and have just updated the IDE to version 1.16.
In the Errata document for IDE 1.16 under target specific issues it says the following:
184869 | ThreadX should not be available on H7 single core, and the build will perform error when threadX is activated |
I am hoping that I have just misunderstood this and there is no issue in using threadx with the stm32h743.
Any feedback very welcome!
Alan
2024-07-26 07:18 AM
Hello,
i am wondering, that this old issue is not answered yet.
This question hits me to, maybe we get an answer soon.
best regards