2015-11-18 04:33 AM
Good morning everyone!
I've been using STM32Cube code generator for a while now. Yesterday I've encountered a problem, while configuring ADC converters using DMA.When I configure one converter with DMA and few channels, everything is ok.But when I add second converter, program eneters some kind of a loop in second converter Start function.I have made a video of the whole process I've gone through. I hope it shows the problem clearly. And here is the code example:2015-11-18 11:20 AM