2023-11-13 11:39 PM
Hi, may i know how do i declare the debug pins (PA13, PA14) as input pins after programming?
Solved! Go to Solution.
2023-11-14 12:32 AM
Hi @Hollis_K ,
The pins PA13 and PA14 can be remapped as input in your application, the same way as for any other GPIOs.
Best regards,
Aime
2023-11-14 12:32 AM
Hi @Hollis_K ,
The pins PA13 and PA14 can be remapped as input in your application, the same way as for any other GPIOs.
Best regards,
Aime
2023-11-14 12:53 AM
If you need to debug and at the same time use these pins for IO operations, it is possible to use the same MCU in a case with more pins and use other GPIOs instead of PA13,14. After debugging the program, change back to PA13,14 and write the debugged program into a small case. It is almost necessary for 8-pin cases.
2023-11-14 5:39 PM
Hi @Aime ,
thanks for the information. After debugged the program, necessary to reset gpio pin if using the debug pins as input pins? There are some reference i find if using debug pins as the gpio output pins:
...
LL_GPIO_SetOutputPin(GPIOA, LL_GPIO_PIN_14);
LL_mDelay(1);
LL_GPIO_ResetOutputPin(GPIOA, LL_GPIO_PIN_14);
LL_mDelay(500);
LL_GPIO_ResetOutputPin(GPIOA, LL_GPIO_PIN_13);
LL_mDelay(1);
LL_GPIO_SetOutputPin(GPIOA, LL_GPIO_PIN_13);
...
if use as gpio input, will it be the same? Curious about that.