Skip to main content
Associate
Feb 5, 2025 2:40 PM UTC
Solved

I2C between two NUCLEO-F446RE boards

Hi, I am trying to use a Nucleo-F446re as master and another one as slave. But the master is probably being timed out (not sure). Can you guys please have a look at my code and configuration. Thanks in advance <3 

 

My Wiring:

1. I connected PB8 & PB9 of both master and slave via direct wire as I used then as SCL and SDA

2. Connected GND of master and slave

 

My code:

Master code:

 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "i2cMaster.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
char msgToSend[] = "MsgFromMaster";
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_I2C1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

int sz = 50;
uint8_t sndData[50];

void writeData(uint8_t* msg, uint8_t len){
	sndData[0] = len;
	memcpy(&sndData[1],msg,len);
	if(HAL_I2C_Master_Transmit(&hi2c1, (0x27 << 1), sndData, len+1, 10000) != HAL_OK){
		sz = 100;
	}
	sz = -1;
}


/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_I2C1_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	 writeData((uint8_t*)msgToSend,13);
	 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 16;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2C1 Initialization Function
 * None
 * @retval None
 */
static void MX_I2C1_Init(void)
{

 /* USER CODE BEGIN I2C1_Init 0 */

 /* USER CODE END I2C1_Init 0 */

 /* USER CODE BEGIN I2C1_Init 1 */

 /* USER CODE END I2C1_Init 1 */
 hi2c1.Instance = I2C1;
 hi2c1.Init.ClockSpeed = 100000;
 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c1.Init.OwnAddress1 = 0;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C1_Init 2 */

 /* USER CODE END I2C1_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : LD2_Pin */
 GPIO_InitStruct.Pin = LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

 

Slave Code:

 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Minimal I2C Slave Example with LED indication (Address: 0x27)
 ******************************************************************************
 * This code sets up an I2C slave that waits for a transmission from a master.
 * The master is expected to send N+1 bytes:
 * - The first byte is the number of payload bytes (N)
 * - Followed by N payload bytes.
 * The onboard LED (LD2) will be lit when the slave is actively listening.
 * When the master starts a transmission, the LED is turned off.
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1; // I2C used for the slave

// Global reception buffer and state variables.
#define BUFFER_SIZE 50
uint8_t rxBuffer[BUFFER_SIZE]; // Buffer for incoming data.
volatile uint8_t rxPayloadLength = 0; // Expected payload length (first byte)
volatile uint8_t rxStage = 0; // 0: waiting for length, 1: receiving payload

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);

/* USER CODE BEGIN 0 */
// For clarity, we'll define helper functions to set the LED state.
void LED_On(void)
{
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
}

void LED_Off(void)
{
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* MCU Configuration--------------------------------------------------------*/
 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();
 MX_I2C1_Init();

 // Enable I2C listen mode (interrupt based) so that the slave responds to address match.
 if (HAL_I2C_EnableListen_IT(&hi2c1) != HAL_OK)
 {
 while(1);
 }
 // Turn the LED on to indicate the device is actively listening.
 LED_On();

 /* Infinite loop */
 while (1)
 {

 }
}

/* --- I2C Slave Callbacks --- */

/**
 * @brief Address Match Callback.
 * Called when the slave address is matched.
 * hi2c: Pointer to the I2C handle.
 * TransferDirection: Direction requested by master.
 * AddrMatchCode: Matched address.
 * @retval None
 */
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
 if (hi2c->Instance == I2C1)
 {
 // Turn off LED when the master starts transmission (i.e. we're no longer just listening)
 LED_Off();

 if (TransferDirection == I2C_DIRECTION_TRANSMIT)
 {
 // Start reception: first, receive one byte (the length)
 rxStage = 0; // Waiting for length byte.
 if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, rxBuffer, 1, I2C_FIRST_FRAME) != HAL_OK)
 {
 while(1);
 }
 }
 else
 {
 // We do not support master reading from slave in this example.
 while(1);
 }
 }
}

/**
 * @brief Slave Reception Complete Callback.
 * Called when the requested number of bytes have been received.
 * hi2c: Pointer to the I2C handle.
 * @retval None
 */
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c)
{
 if (hi2c->Instance == I2C1)
 {
 if (rxStage == 0)
 {
 // First byte (length) received.
 rxPayloadLength = rxBuffer[0];
 rxStage = 1;
 if (rxPayloadLength > 0)
 {
 // Now receive the payload (rxPayloadLength bytes) in the last frame.
 if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, &rxBuffer[1], rxPayloadLength, I2C_LAST_FRAME) != HAL_OK)
 {
 while(1);
 }
 }
 else
 {
 // If payload length is 0, re-enable listening.
 if (HAL_I2C_EnableListen_IT(hi2c) != HAL_OK)
 {
 while(1);
 }
 // Turn the LED on again (active listening)
 LED_On();
 }
 }
 else
 {
 // Payload reception complete.
 // (Data is now stored in rxBuffer[1] to rxBuffer[rxPayloadLength])

 // Re-enable listen mode to accept the next transmission.
 if (HAL_I2C_EnableListen_IT(hi2c) != HAL_OK)
 {
 while(1);
 }
 // Turn the LED on again.
 LED_On();
 }
 }
}

/**
 * @brief I2C Error Callback.
 * Called when an error occurs.
 * hi2c: Pointer to the I2C handle.
 * @retval None
 */
void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *hi2c)
{
 if (hi2c->Instance == I2C1)
 {
 // Attempt to re-enable listen mode in case of error.
 if (HAL_I2C_EnableListen_IT(hi2c) != HAL_OK)
 {
 while(1);
 }
 // Turn the LED on to indicate listening mode is re-established.
 LED_On();
 }
}

/* --- Peripheral Initialization Functions --- */

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 16;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 while(1);
 }

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK |
 RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 while(1);
 }
}

/**
 * @brief I2C1 Initialization Function (Slave)
 * None
 * @retval None
 */
static void MX_I2C1_Init(void)
{
 hi2c1.Instance = I2C1;
 hi2c1.Init.ClockSpeed = 100000;
 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c1.Init.OwnAddress1 = 0x27; // Slave address set to 0x27
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 while(1);
 }
}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* Enable GPIO clocks */
 __HAL_RCC_GPIOB_CLK_ENABLE(); // Adjust if your I2C pins are on a different port.
 __HAL_RCC_GPIOA_CLK_ENABLE(); // For LED if needed (depends on board)

 /* Configure I2C1 SCL and SDA pins */
 /* Adjust the pins if your board uses different ones */
 GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7; // Example: PB6 (SCL) & PB7 (SDA)
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* Configure LED pin (LD2) */
 /* Adjust port/pin names to match your board's configuration */
 GPIO_InitStruct.Pin = LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 __disable_irq();
 while (1)
 {
 // Stay here in case of error.
 }
}

 

 

 

Can anyone please verify why my code is not working ? I am a beginner, trying to make it work for 3 days. I appreciate your attention. Thank you.

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Feb 5, 2025 2:57 PM UTC

@Asif17r wrote:

the master is probably being timed out (not sure). 


So what have you done to confirm whether that is or is not the case?

  • Used an oscilloscope and/or logic analyser to see what's happening on the wires?
  • Used the debugger to see what's happening in the code?

Have you verified that your Master works with a known-good slave?

https://community.st.com/t5/stm32-mcus-products/i2c-communication-between-two-different-stm32-evk-boards/m-p/755042/highlight/true#M268963

 

General debugging tips:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/706966/highlight/true#M49 

 

PS:

Have you tried any of the provided I2C examples:

AndrewNeil_0-1738767911806.png

https://www.st.com/resource/en/application_note/an4739-stm32cube-firmware-examples-for-stm32f4-series-stmicroelectronics.pdf#page=12

https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32446E-Nucleo/Examples/I2C

 

PS:


@Asif17r wrote:

My Wiring:

1. I connected PB8 & PB9 of both master and slave via direct write (sic) as I used then as SCL and SDA

2. Connected GND of master and slave


I guess "write" there means "wire" ?

Note that describing wiring in words never works well - a diagram is far more effective.

You didn't mention pullups?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

9 replies

Andrew Neil
Andrew NeilBest answer
Super User
Feb 5, 2025 2:57 PM UTC

@Asif17r wrote:

the master is probably being timed out (not sure). 


So what have you done to confirm whether that is or is not the case?

  • Used an oscilloscope and/or logic analyser to see what's happening on the wires?
  • Used the debugger to see what's happening in the code?

Have you verified that your Master works with a known-good slave?

https://community.st.com/t5/stm32-mcus-products/i2c-communication-between-two-different-stm32-evk-boards/m-p/755042/highlight/true#M268963

 

General debugging tips:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/706966/highlight/true#M49 

 

PS:

Have you tried any of the provided I2C examples:

AndrewNeil_0-1738767911806.png

https://www.st.com/resource/en/application_note/an4739-stm32cube-firmware-examples-for-stm32f4-series-stmicroelectronics.pdf#page=12

https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32446E-Nucleo/Examples/I2C

 

PS:


@Asif17r wrote:

My Wiring:

1. I connected PB8 & PB9 of both master and slave via direct write (sic) as I used then as SCL and SDA

2. Connected GND of master and slave


I guess "write" there means "wire" ?

Note that describing wiring in words never works well - a diagram is far more effective.

You didn't mention pullups?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Asif17rAuthor
Associate
Feb 5, 2025 5:14 PM UTC

Thank you for those samples. I am new, I have not tried those samples yet. I will try now. 

Do we need pull up resistors? I used the internal one with this line

GPIO_InitStruct.Pull = GPIO_PULLUP;

Is this OK or we need to actually add a pullup resistors ?

As per the diagram, I have not found any diagram website with that chip till now. As a result I could not add the diagram. I just had 3 direct wires,

1. Master SCL -> Slave SCL

2. Master SDA -> Slave SDA

3. Master GND -> Slave GND

That's all.

Also, the master code can send I2C signal when I connect it to LCD display. That means the Master Code is good. But in debug mode I observed it gets timed out when connected to Nucleo-F446re slave.

Let me know what you are thinking. 

Andrew Neil
Super User
Feb 5, 2025 5:24 PM UTC

@Asif17r wrote:

I am new, . 


Just new to the STM32, or new to microcontrollers in general? Programming in general?

 


@Asif17r wrote:

Do we need pull up resistors? I used the internal one with this line. 


Microcontroller internal pullups are too "weak" for reliable I2C - you should always use appropriate external pullups.

https://community.st.com/t5/stm32-mcus-products/stm32g071g8u6tr-trying-to-use-i2c-communication/m-p/769341/highlight/true#M272348

See https://electronics.stackexchange.com/a/473799 for an illustration of the effect of pullup values

 


@Asif17r wrote:

As per the diagram, I have not found any diagram website with that chip till now. As a result I could not add the diagram.


So draw the diagram!

A hand-drawn sketch would be sufficient

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Feb 5, 2025 4:03 PM UTC

Here you can find someone to review your code and jump-start your project going.

 

Asif17rAuthor
Associate
Feb 7, 2025 10:05 AM UTC

 I actually solved the problem. The examples helped me a lot. Thank you.

Andrew Neil
Super User
Feb 7, 2025 10:09 AM UTC

For the benefit of future readers, who may find this while looking for answers to the same problem, please describe what the problem was, and how did you solve it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.