cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210E-Eval + blinking test programm from Keil do not work !!!

roger239955
Associate II
Posted on August 18, 2009 at 13:04

STM3210E-Eval + blinking test programm from Keil do not work !!!

2 REPLIES 2
16-32micros
Associate III
Posted on May 17, 2011 at 13:20

Hi roger,

This example in the default Keil/Uvision installation is for the ''STM3210B-EVAL'' board from ST and not for the board that you have. I highly recommend you to use the latest firmware from our web site if you would like run it on our boards :

http://www.st.com/stonline/products/support/micro/files/stm32f10x_stdperiph_lib.zip

.

Cheers,

STOne-32.

roger239955
Associate II
Posted on May 17, 2011 at 13:20

Here is my technical problems:

1.

I've got STM3210E-EVAL evaluation board from ST company. -

target STM32F103ZE

I've tried to programm it's flash with ULINK-ME USB-JTAG on the base of

simple led blinking test programm.

(Taken from C:\Keil\ARM\Boards\ST\STM32F10x_Eval\Blinky

The flash programming is performing, but I cann't see results -

the programm not functions.

What can I do ?

Is it possible use ULINK-ME USB-JTAG for STM3210E-EVAL board?

2.

The flash programming is performing only to use the download button.

Normaly I can flash the programm by use the debug button. But in this

case it works not.

Some details:

OS : WINDOWS XP

IDE-Version:

µVision3 V3.90

Copyright (c) Keil Elektronik GmbH / Keil Software, Inc. 1995 - 2009

License Information:

LEV USER

COMPANY

LIC=----

Tool Version Numbers:

Toolchain: RealView MDK-ARM Version: 3.80a

Toolchain Path: BIN31\

C Compiler: Armcc.Exe V4.0.0.524 [Evaluation]

Assembler: Armasm.Exe V4.0.0.524 [Evaluation]

Linker/Locator: ArmLink.Exe V4.0.0.524 [Evaluation]

Librarian: ArmAr.Exe V4.0.0.524 [Evaluation]

Hex Converter: FromElf.Exe V4.0.0.524 [Evaluation]

CPU DLL: SARMCM3.DLL V3.80a

Dialog DLL: DARMSTM.DLL V1.43

Target DLL: BIN\UL2CM3.DLL V1.50

Dialog DLL: TARMSTM.DLL V1.43

**************************************************