Posted on May 17, 2011 at 13:24Ok the file (wave)is loaded with the DFU demonstration firmware (STM3210E-EVAL_Demo_NORFlash_V2.0.0.dfu) as bin file. But how do I change the audio file ? It is a binary file. How can i change a wave file to a binary f...
Posted on May 17, 2011 at 13:23Hi I startet examples blinky from KEIL subdirectory Examples\ST\STM32F10xFWLib an it works fine (With STM3210E-Eval and ULINK-ME)! Then i start the example I2S\Interrupt but after flashing (Debug)i have following error...
Posted on May 17, 2011 at 13:20Here is my technical problems: 1. I've got STM3210E-EVAL evaluation board from ST company. - target STM32F103ZE I've tried to programm it's flash with ULINK-ME USB-JTAG on the base of simple led blinking test programm....
Posted on May 17, 2011 at 13:13hallo, can anybody help me. my problem is that the programming of the internal flash on the stm3210e-eval is not possible. i tried to programm with DfuSe V2.2.1 At the first step a can programming the externel NOR-Flas...