2009-08-27 4:32 AM
Filter Coefficient calculation tool for ST's DSP library
2011-05-17 4:20 AM
Can anyone help in letting me know about any free tools on internet that can be used for calculating FIR/IIR filter coefficients for usage with the APIs provided in the ST's DSP library. I have searched on ST's website but didn't found any tools for doing this. I know Microchip provide a tool for their DSP libraries. I don't have MATLAB.
2011-05-17 4:20 AM
hi,
I used following applet which works pretty good:http://www.dsptutor.freeuk.com/FIRFilterDesign/FIRFilterDesign.html
You can also grap the java code and modify the simulated sample frequency that suit your needs. I did it because my sample rate is 40kHz instead of the 8k in the applet. If you have a higher sampling rate you need to do this as this will have an influence on your coefficients too. I injected the calculated coefficients into the fir_16by16_stm32 function of the DSP library and it works pretty good. My application on this is filtering the CAB signal (1380Hz out of the main 50hz) to obtain a stable zero crossing detection. I used 32 tapes to get it done. Calculation time is 7.9 µs which is a nice value considering that the cortex is not a DSP ;) [ This message was edited by: guyvo67 on 22-08-2009 10:32 ]2011-05-17 4:20 AM
Check scilab. It is free and is similar to Matlab.
http://www.scilab.org/2011-05-17 4:20 AM
Hi guyvo67,
How did you converted the coefficients from float format to short format so you use fir_16by16_stm32 function ? merci, Asterix [ This message was edited by: asterix.magigimix on 22-08-2009 23:59 ] [ This message was edited by: asterix.magigimix on 23-08-2009 00:38 ]2011-05-17 4:20 AM
You have to convert the calculated coefficients into fixed point (Q15) notation. [-1 , 1 − 2 exp(15)] -> [-32768,32767] Don't forget to shift your output(32 bit) with 15 to the right.
You find quit a lot articles on the fixed point arithmetic if you google around like the wiki : -G2011-05-17 4:20 AM
Thanks guys for the valuable info! Appreciate your quick response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.