cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 virtual com driver problem

ihouses ihouses
Associate III
Posted on February 21, 2018 at 18:04

How to remove totally the Virtual COM driver for STM32?

The STlink is working but the virtual com doesn-t work and windows 10 can not find driver to the board.

Since the driver is delivered in a .EXE format I can not indicate windows where the driver is and re-installing the driver or try to auto search doesn't solve the problem.

On the other hand the board is working in another windows machine.

1 ACCEPTED SOLUTION

Accepted Solutions
ihouses ihouses
Associate III
Posted on February 23, 2018 at 22:48

Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port

Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.

View solution in original post

1 REPLY 1
ihouses ihouses
Associate III
Posted on February 23, 2018 at 22:48

Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port

Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.