2018-02-21 09:04 AM
How to remove totally the Virtual COM driver for STM32?
The STlink is working but the virtual com doesn-t work and windows 10 can not find driver to the board.
Since the driver is delivered in a .EXE format I can not indicate windows where the driver is and re-installing the driver or try to auto search doesn't solve the problem.
On the other hand the board is working in another windows machine.
Solved! Go to Solution.
2018-02-23 01:48 PM
Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port
Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.
2018-02-23 01:48 PM
Well, finally I solved the problem selecting manually the driver, as Virtual serial port->st com-port
Another problem was that I installed the windows 8 driver in a Windows 7 MAchine. Looks like that when the internal FLASH is opening and windows is showing the STM32 drive that virtual serial com port was stopping.