cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 UART Rx with unknown length

bakhti
Associate II

hi i have a problem with my uart program the thing is i have to determine the buffer size of the rx i'll call it rx_buff now i have multiple reception well different messages sizes some times 50bytes some times 2bytes but the problem is that when sending the 2 bytes the call back doesnt trigger until the full 50bytes are full until the rx_buff is full meaning i have to send the 2bytes message 25 times to get a callback is there a way to receive unknown messages with different length ?

using the stm32H750

thanks in advance

2 REPLIES 2
Danish1
Lead III

If you can guarantee there will be a pause after your 2-byte short message, then you could consider using the "Receiver timeout interrupt" present in the USARTs/UARTs. No I don't know how to do that from ST's software layers; I access the registers directly.

What I tend to do is arrange a DMA-driven circular receive-buffer, and then poll that.

Hope this helps,

Danish

AKall.2
Associate II

No DMA:

Have a buffer with size bigger than your incoming data may be. After init, enable UART RX Timeout by:

HAL_UART_ReceiverTimeout_Config(&huart1,35);// for me, 35=37ms for baud9600
HAL_UART_EnableReceiverTimeout(&huart1);

Then insert your UART ERROR callback and include inside it the RTO:

void HAL_UART_ErrorCallback(UART_HandleTypeDef *UartHandle)
  {
  if(UartHandle.ErrorCode & (HAL_UART_ERROR_RTO)){
    RXcount=UartHandle.RxXferSize-UartHandle.RxXferCount;
    /* Set transmission flag: transfer complete */
    UartReady = SET;
    HAL_UART_Abort_IT(UartHandle);//noise on the line or wrong bytes will cause further OVR ints to 
    //be called after the final RTO causing havoc. END transfer here.
  }
  else{//maybe ovr is set
  }
 }