2024-05-16 07:26 PM
In a contest, which is sponsered by ST, I get the NUCLEO-H503RB MB1814A, which seems like a testing product without mass production. Is it possible to get its block diagram of hardware? Why I ask this is that I may face the problem like its HSE is not working.
2024-05-16 08:56 PM
Hello @sallen and welcome to the ST Community
Here is direct links to the documentation and CAD RESSOURCES of this board.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.