STM32CubeIDE 1.12.0 released
STM32CubeIDE 1.12.0 was released today on st.com as well as an in-tool update patch.
What is new in 1.12.0?
* Microcontroller and board lists aligned with STM32CubeMX v6.8.0
– Added the support for the STM32H5 series microcontrollers
– Added the support for new microcontrollers in the STM32U5 series
– Added the support for the STM32WBA series microcontrollers
– Added the support for one new board related to the STM32G4 series: B-G473E-ZEST1S
– Added the support for three boards related to the STM32H5 series: NUCLEO-H563ZI, NUCLEOH503RB, STM32H573I-DK
– Added the support for three new boards related to the STM32U5 series: STM32U5A9J-DK, NUCLEO-U5A5ZJ-Q, NUCLEO-U545RE-Q
– Added the support for one new board related to the STM32WBA series: NUCLEO-WBA52CG
• Editor improved for project examples
When importing a project example, automatically opens the readme file if it exists
• Data analytics enabled by default
• GCC update enabled
– Updates GCC 11, which is already available on the Eclipse® p2 update site
• Debug
– Address column added to the Live Expressions view
• Code quality
– Added the cyclomatic complexity feature that calculates the function complexity based on the builtprogram
– Added a view to display the complexity of each function included in the program
Main fixed issues
126202 GDB client exits randomly during debug session in CubeIDE on Linux.
139495 ST-LINK GDB server wrongly advertise TrustZone core registers with TZEN=0.
140228 Wrong IP registers displayed in the SFR view.
140494 arm-none-eabi-gdb-py.exe is missing in GNU Tools for STM32 11.3.rel1.20221123-1345 on Windows.
14170 2STM32CubeIDE 1.11.0 completely breaks when the 'Darkest Dark Theme' plugin is installed.
142921 When STM32CubeIDE is launched for the second time, the popus is opened even if the data analysis value is deactivated.
Known issues fixed and problems and limitations
Please refer to the wiki.
Where do I obtain STM32CubeIDE 1.12.0?
https://www.st.com/stm32cubeide
… Or update your current installation of STM32CubeIDE using: Help > Check for updates