2025-05-28 1:08 AM
Hi,
I have been trying to deploy the 66GYMAI1 Camera on the STM32 N657X0Q Nucleo board with the Load and Run mode.
However, there is a problem that I could not solve, which is that the project can not jump from FSBL to APPLI.
Because I am trying to jump from FSBL to APPLI to print something by USART, but it doesn't work.
I would be grateful if someone could check it.
2026-01-12 4:11 AM
Hi,
Which IDE environnement are you using ? Did you try to connect the debug with the software reset mode ?
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.