2017-08-06 9:36 PM
Hello all,
In my project, I'm using the STM32F411CEU6, with a 9.6MHz External TCXO as a clock source. I would like to use the same clock to feed another chip in the board.
I was thinking of using the MCO1 or 2 in order to rout out the 9.6MHz to the other chip.
The other chip XTAL input characteristics are:
Can MCO1 or 2 drive an input load of 150k / 20pF @ 9.6MHz?
Thank you all,
Chen
#stm32f411ceu6 #mco12017-08-06 11:03 PM
hello!
Yes it can drive the 9600 KHZ
At Datasheet @I/O AC characteristics, and @Output voltage characteristics, you can find it.
2017-08-06 11:17 PM
Hi Vangelis,
I did looked at the I/O AC characteristics table, but I wasn't sure that the I/O characteristics also refers to the MCO characteristics.
Anyway, just to be sure...
If I use a 3.3V supply, and OSPEEDRy bits are ''01'', I can reach up to 12.5MHz under 50pF load?
Thanks again!
Chen
2017-08-07 12:57 AM
Great! many thanks!
Chen
2017-08-07 1:42 AM
Hello again
For every GPIO pin (except otherwise specified) the output capability is not depend from internal circuitry but from output driver circuit.
At RM0383 @6.2.10 Clock-out capability, the mco functionality, is just an alternate output function of a GPIO pin.