cancel
Showing results for 
Search instead for 
Did you mean: 

Is STM32 usable in this way?

Hitoshi Ehira
Associate
Posted on July 13, 2017 at 12:49

Dear sirs,

I want to make drive recorder.

I think to use, USB(Mass drive), SD card small, TFT window ,camera(I want many cameras).

I do not want to make a proper product. I want only education or hobby.

I found two products.

1,STM32F4x7

2,STM32F469VIT6

1 is get pic slowly? (I need to 15fps or over) 

2 is employ both camera and TFT?

(I saw two function covered with a data sheet)

In addition, as for 2, are a camera and the LCD interface omitted with 100 pins and 144 pins?

thanks

#stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Tilen MAJERLE
ST Employee
Posted on August 07, 2017 at 10:12

Dear

pa_papa_wolf

‌,

You can use STM32 for USB Mass storage, camera and LCD at the same time.

To give you more info, we need more info about your request such as LCD resolution, camera resolution.

Best regards,

Tilen