cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 lowest current?

Mich1
Associate III
Posted on December 07, 2017 at 16:00

Which STM32 has the actual lowest running current consumption (active from flash)?

#stm32-lowest-current
1 ACCEPTED SOLUTION

Accepted Solutions
9 REPLIES 9
Andrew Neil
Evangelist II
Posted on December 07, 2017 at 16:12

define, 'running' ?

Mich1
Associate III
Posted on December 07, 2017 at 16:18

called 'run mode' in ST datasheet

Mich1
Associate III
Posted on December 07, 2017 at 16:49

I hoped ST could advise a component for a new design but it is true that I can read all STM32 datasheets.

Mich1
Associate III
Posted on December 07, 2017 at 17:08

Unfortunatly, only LDO mode is indicated.

From the STM32L476: 100 μA/MHz run mode (LDO Mode)  39 μA/MHz run mode (@3.3 V SMPS Mode)

But is a good start, thanks a lot.

Posted on December 07, 2017 at 16:32

Well, you can get mA/MHz figures for the core from the datasheets - but the actual running current of the entire chip will depend on what peripherals you use, and how you use them ...

Posted on December 07, 2017 at 16:54

I guess they should be able to tell you the lowest mA/MHz number - but, as noted, there's a lot more to it than just that!

Have you spoken to you local FAE and/or Distributor?

Posted on December 07, 2017 at 16:57

http://www.st.com/en/development-tools/st-mcu-finder.html

 

http://www.st.com/content/st_com/en/product-selector.html

 - indeed there is a column for mA/MHz !
Posted on December 07, 2017 at 17:03

Ok, but how much horse power does your application need? Can it sleep a lot?

Most power tends to be consumed by the stuff you have attached to the STM32 parts.

The L0 series runs at some of the lower speeds, and has the least number of gates.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 11, 2017 at 09:04

Hello,

Regarding STM32 MCUs, which consume the smallest current consumption in RUN mode, I would like to highlight two families:

http://www.st.com/en/microcontrollers/stm32l0-series.html?querycriteria=productId=SS1817

based on Cortex-M0+ and

http://www.st.com/en/microcontrollers/stm32l4-series.html?querycriteria=productId=SS1580

based on Cortex-M4F. These two families are defenitely the best in whole STM32 portfolio in terms of current consumption (including RUN mode).

In both families I would propose to focus on devices, which have small amout of resources, especially memory (Flash, SRAM), as this factor has impact on current consumption. In STM32L0 family such devices are

http://www.st.com/content/ccc/resource/technical/document/datasheet/42/c0/ab/e5/71/7a/47/0b/DM00206508.pdf/files/DM00206508.pdf/jcr:content/translations/en.DM00206508.pdf

. Theys can consume the current down to 76 uA/MHz in RUN mode. In STM32L4 family by using the same approach we should select

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/83/b3/60/f6/b1/cc/47/7e/DM00257211/files/DM00257211.pdf/jcr:content/translations/en.DM00257211.pdf

. Here the smallest expected consumption is 84 uA/MHz in RUN mode.

Additionally some of STM32L4 MCUs support a SMPS, which allows to bypass the embedded LDO and reduce the consumption even more. For example

http://www.st.com/content/ccc/resource/technical/document/datasheet/f7/a0/fc/27/24/4e/4f/3f/DM00257192.pdf/files/DM00257192.pdf/jcr:content/translations/en.DM00257192.pdf

, with SMPS, will consume only 36 uA/MHz in RUN mode.

Regards

Szymon