cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 GDB server from STMicro

halherta2
Associate II
Posted on February 16, 2012 at 18:49

I've been playing with the STM32F4Discovery board and I must say that I'm very impressed! I downloaded the ST-LINK utility software from ST micro's website and it works great for downloading.

I just wanted to say that it would be nice if STMicro would include their own GDBserver (with versions for Windows, Linux and possibly Mac OSX) and make it freely available to standardize the debugging software for the STLINK / V2 hardware.

 

I realize that that GDB servers for linux and windows are available from Texane and Atollic...and I have used them...but it would be better if one was available from the company that made the debugger hardware in the first place.

Thank you

 
1 REPLY 1
sjo2
Associate II
Posted on February 22, 2012 at 13:01

Also worth mentioning

http://openocd.sourceforge.net/

now supports the stlink.

Cheers

Spen