cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 MMC compatibility: 4.2 or 4.1?

ned
Associate
Posted on February 21, 2012 at 22:16

In the reference manual (section 26.1) it says:

The SDIO features include the following:

 

? Full compliance with MultiMediaCard System Specification Version 4.2.

 

Card support for three different databus modes: 1-bit (default), 4-bit and 8-bit

but later, in Note 2, we see the odd sentence:

The current version of the SDIO supports only one SD/SDIO/MMC4.2 card at any one time and a stack of MMC4.1 or previous.

 

Why does it specify ''a stack of MMC4.1 or previous''?

There were some major changes between the MMC4.1 and MMC4.2 specifications; one very important one was that 4.2 added the ability to specify addresses using 32-bit sector numbers instead of 32-bit byte addresses.

Can someone explain how the SDIO is fully compliant with the MMC spec 4.2 but not with an MMC 4.2 stack?

Thanks...

#stm32f4-mmc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0