Posted on February 25, 2013 at 13:33Another website that has been designed by marketing :) Anyway it seems that the software can be downloaded from the STVP page but not the STVD page - figure that one out.http://www.st.com/st-web-ui/static/active/e...
Posted on July 31, 2012 at 10:28
This is infact even simpler, just use the following:
openocd -f /usr/local/share/openocd/scripts/board/stm32vldiscovery.cfg
personally i just create a openocd.cfg file and add the following:
...
Posted on July 04, 2012 at 10:27Just to keep things in the same place, OpenOCD can also be used to program/debug using the STLINK/V1 and STLINK/V2http://openocd.sourceforge.net/ Spen
Posted on July 04, 2012 at 10:16STLink support is available in OpenOCD now, this works with STLINK/V1, STLINK/V2 and the various discovery boards.http://openocd.sourceforge.net/ Spen