cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 - FMC and 16b SDRAM but 8b bus

Jda S.1
Associate

Grettings,

Can the FMC be configured to handle a similar configuration?

0693W00000Stn4YQAR.pngI have an SDRAM that has byte enable pins to the upper and lower bytes (Disable -> High Z), but no pins available to map the 16 bits. So, at the moment I'm working with half the memory capacity

0693W00000Stn5gQAB.png 

Can the byte enable be used for this purpose in the FMC of the STM32?

1 REPLY 1

Can't you just be specific about the part(s) you're using instead of illustrating two that you aren't?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..