2015-08-23 8:08 AM
STM32 F7 running hotter than F4?
2015-08-24 5:56 AM
Hi chen.lee.001,
The question you asked on the title of your post cannot give us a clear idea about the problem you are facing or the information you are looking for.Could you please provide more details?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-08-24 7:59 AM
A quick glance to STM32F756 and STM32F439 datasheets: the former consumes around 150mA at the ''everything ON'' setting at 180MHz (and can go higher, both in frequency and power consumption), the latter consumes around 100mA.
Provided similar thermal dissipation, the 'F7 is bound to run hotter... JW2015-08-25 6:36 AM
It is claimed that the F7 chip has the same power consumption as the F4. Maybe ST guys can shed some light on this.
I ordered one Discovery board to further evaluate. Anyone has any experience or observation on this?