cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 CubeMX Installation Problems Mac

Jean-Marc Sujata
Associate
Posted on April 27, 2017 at 14:46

Hi everyone,

I turn to you in complete despair. I thought I would start tonight with My Nucleo, but couldn't even get past the Installation of the CubeMX software. When I double click on the app (SetupSTM32CubeMX-4.20.1) or open it via left click and open, I get the message: 

“SetupSTM32CubeMX-4.20.1� is an application downloaded from the Internet. Are you sure you want to open it?'

as usual. But after clicking on open, nothing happens. I also tried to execute it via terminal as suggested by another post, but get:

Jean-Marcs-MacBook-Pro-2:A Joeme$ java -jar SetupSTM32CubeMX-4.20.1.app

Invalid or corrupt jarfile SetupSTM32CubeMX-4.20.1.app

Does someone know how to solve this? Thank you in advance!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
john doe
Lead
Posted on April 28, 2017 at 19:19

the mac installer is broken and has been for many versions.

dont try to launch the .app, launch the .exe with the java -jar command.  you will also need to use sudo to do it because it installs in the applications folder

View solution in original post

3 REPLIES 3
Imen.D
ST Employee
Posted on April 27, 2017 at 18:59

Hi,

Are you following the instructions in this

http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM00104712.pdf/files/DM00104712.pdf/jcr:content/translations/en.DM00104712.pdf

 manual to install STM32CubeMX in command-line mode and install the software requirements as Java Development Kit 1.7.0_45 ?

You should make sure that you have administrator rights.

0690X00000606swQAA.png
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Max
ST Employee
Posted on April 28, 2017 at 05:51

You may want to update Java.

Also, try downloading again, your file may be corrupted.

john doe
Lead
Posted on April 28, 2017 at 19:19

the mac installer is broken and has been for many versions.

dont try to launch the .app, launch the .exe with the java -jar command.  you will also need to use sudo to do it because it installs in the applications folder