2020-03-16 8:31 AM
Customer asks me to use STM32 powered from 3.3V with ADC reference 3.3V too (different source). So there is two possibel topologies:
In the DS I didnt found clear info about this:
"A maximum difference of 300 mV between VDD and VDDA can be tolerated during power-up and power-down operation"
"VDDA Must be the same potential as VDD"
"The voltage on VREF+ may range between 2.4 V and VDDA"
In my case, standard 3.3V source can differ +/-200mV from reference 3.3V source. Is it acceptable to use STM32F405 this way?
2020-05-19 8:20 AM
Hello @LSind.1
Connect VDD and VDDA, use precision source for VREF but make sure that VREF < = VDDA
For more details about ADC characteristics refer to table 67 in the STM32F405 datasheet DocID022152 Rev 8
Best regards
Bouraoui