2018-03-03 4:24 AM
Hello
I would like to program a stm32vldiscovery from Linux.
Unfortunately, the board has a STLink V1 embedded. Is it possible to upgrade a STLink to STLink/V2?
Or is it possible to directly flash the board with an external STLink/V2?
Bests
Cedric
Solved! Go to Solution.
2018-03-05 8:45 AM
Because I am using Linux, v1 is not compatible
2018-03-05 8:50 AM
2018-03-13 2:40 AM
It works fine with texane/stlink. Thanks a lot.